SABRE AI SPI NOR Flash update issue via uuu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE AI SPI NOR Flash update issue via uuu

1,132 Views
tamas_szucs
Contributor I

Hi All,

I'm trying to use uuu to write u-boot to SPI NOR Flash.

S1, S2 and J3 are configured to boot Serial NOR Flash on CPU card.

I'm attaching output from uuu.

Any pointers are welcome.

Thanks,

Tamas

0 Kudos
Reply
1 Reply

1,017 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Tamas,

The i.MX6 SABRE-AI does not have eMMC on board, so, you could try with a different boot option (like a SD card).

Anyway, please consider that you need to download the root file system, and a specific U-Boot for any platform / boot option, like the described on the following thread:

i.MX6qp Sabre AI cannot boot the validation sdcard image 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply