SABER i.MX 7Dual J30 connector

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABER i.MX 7Dual J30 connector

4,341件の閲覧回数
chadwagner
Contributor I

I am looking for the part number for the "J30" port for MIPI DSI display connector (BTB Connector,socket,Right Angle,24Pin,0.4MM Pitch,1.5MM Height,Au,Black,SMD) on the SABER i.MX 7Dual board.

A more detailed list of the BOM would be great.

ラベル(1)
タグ(1)
0 件の賞賛
返信
13 返答(返信)

3,867件の閲覧回数
eric_kang
Contributor II

I know the J30 connector is "DF40C-24DS-0.4V(51)".

You can confirm the connector in the below site.

https://community.nxp.com/message/1009994?commentID=1009994#comment-1009994

0 件の賞賛
返信

3,867件の閲覧回数
chadwagner
Contributor I

Any help to get this display working would be appreciated.

Thanks.

0 件の賞賛
返信

3,867件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the Eric post, which is the same information I got from development team:

The connector manufacture’s part number is: DF40C-24DS-0.4V(51)

0 件の賞賛
返信

3,867件の閲覧回数
chadwagner
Contributor I

Will the TFT3P5581-T also work?

0 件の賞賛
返信

3,867件の閲覧回数
chadwagner
Contributor I

I got the TFT3P5581-T. It is the TFT3P5581-E with a touch screen. The connector for the touch screen does not appear to have a place to connect to the SABRE i.MX 7Dual. I would love more information on this display to make it power up and I still need the connectors to connect everything on my custom board.

0 件の賞賛
返信

3,867件の閲覧回数
chadwagner
Contributor I

I still need the part number to connect to my proto type display. Can you please ask the engineering team for this part number?

0 件の賞賛
返信

3,867件の閲覧回数
chadwagner
Contributor I

The description in the Excel BOM from the "Design files for i.MX 7Dual" is still "Connector,Audio Jack,Right Angle,3.5MM Plug Diameter,Gold Flash 1u,Pink,DIP"?

0 件の賞賛
返信

3,867件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I checked J29, yes for J30 we don't offer part number, I checked this connector and discussed with hardware engineer, we think you need to decide which mipi dsi you use, then you can get the matched connector, you don't need to know mipi dsi connector part number on imx7d board  .

0 件の賞賛
返信

3,867件の閲覧回数
chadwagner
Contributor I

To try the connector on the board I need to make an adapter board which needs that part number. A more complete list of all the parts would be great. We want to make a custom version of the board in the future, but we need to ensure the i.MX can do everything we need first.

0 件の賞賛
返信

3,867件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the imx7d-sdb-mipi-dsi.dts in the bsp, the imx7 supports TRULY-WVGA-TFT3P5581E display, then I got information that the TFT3P5581-E connects directly to the MX7 Sabre board 

0 件の賞賛
返信

3,867件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

3,867件の閲覧回数
chadwagner
Contributor I

The BOM list the part as “BTB Connector,socket,Right Angle,24Pin,0.4MM Pitch,1.5MM Height,Au,Black,SMD” which is not enough detail to order the part.

0 件の賞賛
返信

3,867件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the BOM file I sent to you:

"BTB Connector,Socket,AXT530124,30Pin,0.4MM Pitch,without bosses,Height 1.0mm,Ni+Au,panasonic,SMD"

 the AXT530124 is part number

0 件の賞賛
返信