[S32R294] SPT enable issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[S32R294] SPT enable issue

1,715 次查看
GaryKuo
Contributor I

Hi Sir,

I' m testing with S32R294 EVB board (v1.1).

When I tried to initialize SPT, I got `RSDK_SPT_RET_ERR_HW_RST` error state.

This is because pSptRegs->CS_STATUS3.B.PROC_STATE is 0, so that  CheckSptRst() in SptConfigHw() return RSDK_SPT_RET_ERR_HW_RST.

But when I try RSDK_offline_example, I found `pSptRegs->CS_STATUS3.B.PROC_STATE` is "1" in  SptConfigHw() and can success pass initial process.

Is there anything I should enable before SPT is launched?

Can you suggest me how to solve this issue?

 

Thank you,

Gary

标记 (1)
0 项奖励
回复
2 回复数

1,653 次查看
GaryKuo
Contributor I

Hi,

I've solved this issue, thank you.

Gary

0 项奖励
回复

1,660 次查看
b41937
NXP Employee
NXP Employee

Hi,

Can you provide some context in which this error occurs? It would help if we can reproduce the issue but my understanding is that the provided examples work. 

0 项奖励
回复