S/W encoding H.264 with i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S/W encoding H.264 with i.MX7D

Jump to solution
959 Views
ScottKerstein
Contributor III

Hello,

Looking to encode H.264 from a 1080p30fps imager on the i.MX7D using GStreamer.  Is there a way to determine the CPU utilization and if a Cortex-A7 running at 1.2GHz is enough to do this task?  This is the only task.  

Thanks, in advance.

Scott

Labels (4)
0 Kudos
1 Solution
811 Views
ScottKerstein
Contributor III

Thanks, Igor.  Looks like it will be limited to just JPEG in software.

View solution in original post

0 Kudos
2 Replies
811 Views
igorpadykov
NXP Employee
NXP Employee

Hi Scott

nxp linux video performance without vpu is described in attached Release Notes

Table 31. Video codec specification for hardware without VPU acceleration.

More details about VPU versus non-VPU analysis  can be obtained creating service request

Support|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
812 Views
ScottKerstein
Contributor III

Thanks, Igor.  Looks like it will be limited to just JPEG in software.

0 Kudos