Running Free RTOS and Linux simultaniously on an iMX 6Dual(Lite/Plus)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running Free RTOS and Linux simultaniously on an iMX 6Dual(Lite/Plus)

ソリューションへジャンプ
1,478件の閲覧回数
jeroenvanderlaa
Contributor III

We are thinking about switching from the iMX 6SoloX to an iMX 6Solo MCU. There was only 1 application that needed the M4 core for FreeRTOS. There is a lot of documentation on running FreeRTOS on the M4 while running Linux on the A9 core. Is it possible to run Linux on cpu0 and FreeRTOS (or another instance of Linux) on cpu1 on an iMX 6Dual(X)? This means we could upgrade a few boards for that specific application while running the rest on a Solo processor.

Best regards,

Jeroen van der Laan

タグ(1)
0 件の賞賛
返信
1 解決策
1,283件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Basically it is possible - to run different OS(s) on different cores, using hypervisor,
but we do not have any examples for i.MX6.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

元の投稿で解決策を見る

2 返答(返信)
1,284件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Basically it is possible - to run different OS(s) on different cores, using hypervisor,
but we do not have any examples for i.MX6.

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

1,283件の閲覧回数
jeroenvanderlaa
Contributor III

Thanks,

that might do the trick.

0 件の賞賛
返信