Run "weston-simple-egl" failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run "weston-simple-egl" failed

1,790 Views
raybloodworth
Contributor II

Hi,

   I'm running weston with these steps : Building Wayland-Weston for i.MX6

   In the wayland terminal, I enter 'clients/weston-simple-shm' and i could see a scrolling color pattern.

   But it is failed when i enter 'clients/weston-simple-egl'.

   The terminal shows someinfomation:

     [1]HAL user version 4.6.9 build 6622 Aug 16 2013 11:28:30

     [2]HAL kernel version 4.6.9 build 1210

     Segmentation fault (core dumped)

   kernel version : L3.0.35_4.1.0

   GPU-VIV : gpu-viv-wl-bin-mx6q-3.0.35-4.1.0

Could anyone tell me what's the problem?

Labels (2)
0 Kudos
Reply
2 Replies

921 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

You should try the latest L3.10.17_1.0.0   BSP version, where this bug is fixed and includes a new version of vivante driver .

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

hope this helps

0 Kudos
Reply

921 Views
jamesbone
NXP TechSupport
NXP TechSupport

Bio_TICFSL,  Can you please comment?

0 Kudos
Reply