Run hello world application using SD card for i.MX RT1064 Evaluation Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run hello world application using SD card for i.MX RT1064 Evaluation Kit

Jump to solution
1,347 Views
Jayadev
Contributor I

Hello,

I followed Getting Started with MCUXpresso SDK for EVK-MIMXRT1064.pdf and was able to run hello world application using MCU Xpresso IDE. Now I want to flash the same program onto an SD card and run the application on boot. Is there a way to do that?

Also MCUXpresso SDK for EVK-MIMXRT1064.pdf, to Run a demo using Arm GCC has steps only for Windows OS. My system is ubuntu and I have installed toolchain. Are there any steps on how to proceed further?

0 Kudos
Reply
1 Solution
1,320 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Jayadev,

Please look into the following knowledge base article as I believe it will prove very useful for your inquiry: https://community.nxp.com/t5/Blog/Tutorial-Booting-the-NXP-i-MX-RT-from-Micro-SD-Card/ba-p/1131074

If you have further questions about this topic, do let me know.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
3 Replies
1,228 Views
Jayadev
Contributor I

Hi @everyone,

I got the output on the terminal by doing a reset after you boot up board in SD card mode. Thank you for the support.

BR,

Jayadev.

0 Kudos
Reply
1,271 Views
Jayadev
Contributor I

Hi @EdwinHz 

I followed the tutorial and was able flash image successfully. But SD card seems to be empty. And I am not able to see hello world in Putty.

I also checked these discussions,

https://community.nxp.com/t5/i-MX-RT/RT1050-EVK-Boot-from-SD-Card-to-ITCM/m-p/722529

https://community.nxp.com/t5/i-MX-RT/SD-card-flashing-and-booting-in-i-MXRT1050-EVK/m-p/775741

My start address is 0x1000. But I am not able to see the output. I am attaching my cfg.ini files and imx-itcm-unsigned.zip. I would appreciate any help provided.

0 Kudos
Reply
1,321 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Jayadev,

Please look into the following knowledge base article as I believe it will prove very useful for your inquiry: https://community.nxp.com/t5/Blog/Tutorial-Booting-the-NXP-i-MX-RT-from-Micro-SD-Card/ba-p/1131074

If you have further questions about this topic, do let me know.

BR,
Edwin.

0 Kudos
Reply