Rpmsg enabling patch file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Rpmsg enabling patch file

跳至解决方案
1,808 次查看
arunsathian
Contributor III

Hi,

Is the attached patch file suitable for L5.10 also? 

or else what are the changes need to be done in this patch file.

0 项奖励
回复
1 解答
1,709 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @arunsathian 

You can refer  AN5317 Loading Code on Cortex-M from U-Boot/Linux for the i.MX Asymmetric Multi-Processing Application Processors 

https://www.nxp.com/docs/en/application-note/AN5317.pdf

 

Best Regards

Zhiming

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,798 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @arunsathian 

You can't use it directly, there are lots of changes in framework and dts.

 

1,791 次查看
arunsathian
Contributor III
Hi @Zhiming_Liu
what are the changes need to be done in this patch file?Can you please explain in a brief?
0 项奖励
回复
1,784 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The device tree changes a lot(arch/arm64/boot/dts/freescale/imx8qxp-mek-rpmsg.dts), and L5.10 don't use rpmsg driver anymore, it uses remoteproc framework.

1,735 次查看
arunsathian
Contributor III
Hi @Zhiming_Liu
Are you saying that for L5.10 version we strictly need to use remoteproc instead of rpmsg?
If do so can you please share any documents related with it.
0 项奖励
回复
1,710 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @arunsathian 

You can refer  AN5317 Loading Code on Cortex-M from U-Boot/Linux for the i.MX Asymmetric Multi-Processing Application Processors 

https://www.nxp.com/docs/en/application-note/AN5317.pdf

 

Best Regards

Zhiming

0 项奖励
回复