Rewind feature using gstreamer, abruptly rewinds to the start of the stream

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rewind feature using gstreamer, abruptly rewinds to the start of the stream

1,009件の閲覧回数
shwetha
Contributor I

Hi,

I am developing a basic Gstreamer based audio player which is expected to support play, pause, seek, fast forward, rewind and stop functionalities. I am facing some issues in the rewind feature on imx6. 

When I test the rewind feature on my desktop, there is no issue and behaves as expected (gradually rewinds to the start of the stream at some steady rate). But, the problem is when I test the rewind functionality on the target(imx6), it abruptly skips to the start of the stream and the pipeline moves to the STOP state. I am not able to understand what is going wrong. Is there something extra that I need to take care while executing on the board? All other features are working perfectly fine.

ラベル(3)
タグ(2)
0 件の賞賛
返信
0 返答(返信)