Returning an IMX8X to NXP for debug, and the effects of Partial Field Return Lifecycle State

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Returning an IMX8X to NXP for debug, and the effects of Partial Field Return Lifecycle State

1,600 次查看
wdcrith
Contributor II

Hello NXP,

Two questions for you.

First, if I ever need to return an IMX8X processor to NXP for debugging, what interfaces (JTAG, SDP, etc) need to be available on my board (if any)?

And a second related question, I know that there is a lifecycle state for "Partial Field Return" though the details are pretty sparse for what this lifecycle actually does. What interfaces will be enabled by moving the IMX8X device to the Partial (OEM) Field Return state?

Thanks.

0 项奖励
回复
4 回复数

1,577 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @wdcrith ,

I hope you're doing well! 

Let me double check with our team about interfaces for debugging boards.

Regarding Lifecycle States, there's Section 2.1.4.1.1 Chip Life Cycle in the Security Reference Manual (https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX8QXPSRM&appType=moderatedWithout...).

Thank you.

Best regards,
Hector.

 

0 项奖励
回复

1,541 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @wdcrith ,

For debugging boards we recommend having USB, JTAG and UART available. 

Best regards,
Hector.

0 项奖励
回复

1,525 次查看
wdcrith
Contributor II

Thanks for the replies Hector,

Based on the SRM, I'm assuming the Partial Field Return lifecycle state will only affect the enforcement of the AHAB, and opening up the JTAG for debug.

On my device I disable SDP (Serial Download Protocol over USB) at the same time as closing the AHAB. Does Partial Field Return override or re-enable SDP?

 

And for the peripherals for debugging, I believe I could expose JTAG and UART for NXP to use. USB may be unavailable (depending if SDP gets re-enabled). Is JTAG + UART enough for NXP to do their debugging activities?

0 项奖励
回复

1,449 次查看
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @wdcrith ,

I hope you're doing great!

It is highly recommended to have all three ports available for debugging, not having one and sending it over would be by your own risk. 

I don't believe partial field return state enables SDP back since they are different fuses. 

Best regards,
Hector.

0 项奖励
回复