Resume from standby doesn't work for UART4 on i.mx7D Sabre board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Resume from standby doesn't work for UART4 on i.mx7D Sabre board

513 Views
robertopozzi
Contributor I

I have an imx7D Sabre board on which I have actived the UART4 ( available on mikro BUS).

The UART4 works perfectly ( I can send/receive data to a PC)

Before sending the board to standby I enable the wakeup from UART4 sending by the console the following comand:

echo enabled > /sys/bus/platform/drivers/imx-uart/30a70000.serial/tty/ttymxc4/power/wakeup

then I put the board in standby with the command:

echo standby > /sys/power/state

Sending then some bytes to the UART4, the  Sabre board doesn't wake up.

Instead the wake up works fine from the console.

Console Enable wakeup comand used:

echo enabled > /sys/bus/platform/drivers/imx-uart/30860000.serial/tty/ttymxc0/power/wakeup

Have I forgotten some  further setting to enable the Wakeup from standby for the  UART4?

Roberto Pozzi

Labels (1)
0 Kudos
Reply
1 Reply

426 Views
igorpadykov
NXP Employee
NXP Employee

Hi Roberto

could you try latest L4.9.11 bsp described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

and try to add "wakeup-source" to dts, as described

in linux/Documentation/devicetree/bindings/power/wakeup-source.txt

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply