Restriction of i.MX8QXP 24MHz XTAL Cload value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Restriction of i.MX8QXP 24MHz XTAL Cload value

跳至解决方案
1,063 次查看
mamorukanou
Contributor IV

Hi,

Are there some restriction of i.MX8QXP Xtal CLoad.

According to the data sheet 4.4.1 OSC24MHz, i. MX8QXP internal XTAL circuit has integrate trimmable internal loading capacitors.
So we understand that we can use any 24MHz Xtal which has any Cload value.

The data sheet says Typ CL 18pF, but we will connect  EPSON TSX-3225 (CL=9pF, 9pF smaller) and i.MX8QXP directly without extra capacitor. 

Are there any problems?

Best Regards,

kanou

0 项奖励
回复
1 解答
988 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Kanou,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your NXP FAE/Sales or with your DBM.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
989 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Kanou,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your NXP FAE/Sales or with your DBM.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 项奖励
回复
988 次查看
mamorukanou
Contributor IV

Hi Carlos,

Thank you for quick response.

OK, I'll ask NXP Japan FAE team.

BR,

kanou

0 项奖励
回复