Restriction of i.MX8QXP 24MHz XTAL Cload value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Restriction of i.MX8QXP 24MHz XTAL Cload value

Jump to solution
1,082 Views
mamorukanou
Contributor IV

Hi,

Are there some restriction of i.MX8QXP Xtal CLoad.

According to the data sheet 4.4.1 OSC24MHz, i. MX8QXP internal XTAL circuit has integrate trimmable internal loading capacitors.
So we understand that we can use any 24MHz Xtal which has any Cload value.

The data sheet says Typ CL 18pF, but we will connect  EPSON TSX-3225 (CL=9pF, 9pF smaller) and i.MX8QXP directly without extra capacitor. 

Are there any problems?

Best Regards,

kanou

0 Kudos
Reply
1 Solution
1,007 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kanou,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your NXP FAE/Sales or with your DBM.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,008 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kanou,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your NXP FAE/Sales or with your DBM.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply
1,007 Views
mamorukanou
Contributor IV

Hi Carlos,

Thank you for quick response.

OK, I'll ask NXP Japan FAE team.

BR,

kanou

0 Kudos
Reply