Dear All,
I am using PF3001 for restart application. I controlled the PMIC_ON_REQ of pmic chip by configure the SNVS_PMIC_ON_REQ from my imx processor. And also I enabled the PWRONRSTEN and RESTARTEN bit in PWRCTRL register of PMIC chip as per datasheet.
As per datasheet after 4 Seconds the PMIC will restart. But, in my case there is no restart. I got result like the processor is off(the software is off) and the hardware side the voltage was low.
Regards,
VinothS
Solved! Go to Solution.
Actually, this restart logic as described for the RESTARTEN bit does not work since it contradicts with the functionality of the PWRON signal. So, the ON/OFF state of PMIC is completely controlled only by the PWRON signal.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Actually, this restart logic as described for the RESTARTEN bit does not work since it contradicts with the functionality of the PWRON signal. So, the ON/OFF state of PMIC is completely controlled only by the PWRON signal.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur,
Thanks, I done through software.