Reset pin on JTAG unavailable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset pin on JTAG unavailable

493 Views
vivekvix
Contributor II

vivekvix_0-1702548918187.png

The above image shows the JTAG pins from the IMX8MP Processor

vivekvix_3-1702548984954.png

The above shows the image of the JTAG connector which we are using, which contains the RESET pin. 

We have used the NXP provided pin config tool, but the reset pin for the same is not available.
The image for which is also attached below. 
Pls note that there is no JTAG_RESET on the IMX8mp whereas there is a JTAG_RST on the connector.

vivekvix_2-1702548929738.png

 

What is the reset mechanism used for resetting while using JTAG?
Please provide us the solution for the same

 

0 Kudos
Reply
2 Replies

470 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

460 Views
vivekvix
Contributor II

I have gone through the link
But it shows how nRST can be used for boundary scan. 

I want to know how the reset functionality can be implemented...

0 Kudos
Reply