Hi all
My customer will start a development for first prototype and want to confirm about requirement of operating range with i.MX6SL.
Does user must to satisfy a following requirement ?
(The requirement is described in IMX6SLCEC)
「VDD_ARM_IN and VDD_SOC_IN must be at least 125 mV higher than the LDO Output Set Point for correct voltage regulation.」
They measured CPU's core voltage levels with SABRE-EVK. But EVK doesn't satisfy the requirement.
Please see a following table.

Why EVK doesn't satisfy the requirement ?
NXP suppose that EVK is only for emulation use, so EVK deosen't satisfy the requirement.
Is it correct ?
As a result, user must set following register value to satisfy the requirement by themselves.
Is it correct ?
REG2_TARG
REG1_TARG
REG0_TARG
Ko-hey