Required timing model (.v) for LPPDR4 simulation using Hyperlynx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Required timing model (.v) for LPPDR4 simulation using Hyperlynx

1,494 次查看
aprakashbaler
Contributor I

I am simulating for SI in hyperlinx for LPDDR4 interface at 4000mbits/s. there are failuers in max slew rate for all the drive strength and ODT configurations for Data write cycle. 

Required timing model or any solution to reduce the slew rate. 

Regards

Avinash B P

标记 (3)
0 项奖励
回复
3 回复数

1,461 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the device that you are testing?
Also, which verion of the IBIS file you are using?

Best regards/Saludos,
Aldo.

0 项奖励
回复

1,439 次查看
aprakashbaler
Contributor I

Hello Aldo,

 

Device i am using is MIMX8ML8CVNKZAB.

and the IBIS used is ibis_imx8mp_v2_20201023.

Regards

Avinash B P

0 项奖励
回复

1,339 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

max slew rate failures are not seen as a high risk. We recommend for customers follow our Hardware Developer's Guide and good design practices. And that should be enough.

Best regards/Saludos,
Aldo.

0 项奖励
回复