Required Documents related to create Android Application APK for IMX8MM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Required Documents related to create Android Application APK for IMX8MM

1,235 次查看
Ruban1
Contributor II

Required Documents related to create Android Application APK for IMX8MM.

How to access from application the hardware like GPIO, I2C, UART etc .

How to execute su command from Application APK.

Kindly provide every related documents for accessing NXP IMX8MM from Android Application APK.

Thanks and Regard

Ruban

标签 (1)
0 项奖励
回复
2 回复数

1,224 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

You may refer to the google documentation for this, please check the following link:
https://developer.android.com/


Best regards,
Aldo.

0 项奖励
回复

1,218 次查看
Ruban1
Contributor II

I have built application to access the GPIO pin but i am not able to but if i am connecting to Putty and using command line .. And type su command which goes to the root permisssion then only i am able to access the gpio. But due to i am using Android I have to access through application layer only . I am not able to provide even run time command as su.

Any one sample code Application is also fyn .I can build Application having reference to that .But the Sample should be purely with respect to NXP imx8mm board only.. Because i try with digi, tordex, vardin, varsitice.. Those application is not supporting to our nxp imx8mm.

Kindly provide more details

Thanks and Regards

Ruban

0 项奖励
回复