Require DRAM support for i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Require DRAM support for i.MX6ULL

Jump to solution
603 Views
mrudangshelat1
Senior Contributor II

Hi karinavalencia‌ and dgd‌,

In one of the ongoing medical project, we have used i.MX6ULL. And based on datasheet it supports LPDDR2, DDR3, DDR3L. We have used the MCP package of eMMC+LPDDR2 due to form factor constraints in our design. Now the existing MCP package of eMMC+LPDDR2 is EOL. And they have availability only with eMMC+LPDDR3.

Does i.MX6ULL can support LPDDR3 with extra SW effort? If yes, kindly provide the solution.

Else provide the other optional solution. 

Kindly discuss this with your team and provide the answers as soon as possible.

Regards,

Mrudang

Labels (1)
Tags (1)
1 Solution
519 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

unfortunately i.MX6ULL does not support LPDDR3, no software workaround available, sorry.

Supported  DDR3(L)/LPDDR2 as described in Chapter 35 Multi Mode DDR Controller (MMDC)

i.MX 6ULL Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
520 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

unfortunately i.MX6ULL does not support LPDDR3, no software workaround available, sorry.

Supported  DDR3(L)/LPDDR2 as described in Chapter 35 Multi Mode DDR Controller (MMDC)

i.MX 6ULL Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

519 Views
mrudangshelat1
Senior Contributor II

Hi Igor,

thanks for the confirmation.

Mrudang

0 Kudos