juangutierrez Oct 1, 2013 9:40 AM (in response to jamesbone)
My initial guess is that setting the forceIPicture parameter is in the right way.
I or Intra frames are those one which are encoded regardless of the previous frames.
There is no prediction involved.
I guess keyframe refers to this type of I-frame
This is the description of the forceIPicture EncParam from the vpu_api_reference manual:
"If this value is 0, the picture type is determined by the VPU according to the
various parameters such as encoded frame number and GOP size.
If this value is 1, the frame is encoded as an I-picture regardless of the frame
number or GOP size, and I-picture period calculation is reset to the initial state.
For MPEG-4 and H.263, I-picture is sufficient for decoder refresh. For H.264
mode, the picture is encoded as an Instantaneous Decoding Refresh (IDR) picture.
This value is ignored if skipPicture = 1."