Request for signing barebox on phytec phycore imx6 card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for signing barebox on phytec phycore imx6 card

803 Views
haGkiu
Contributor I

Hello Community,

I am working on implementing secure boot on an imx6 phytec phycore card.

I used cst 3.3.0 to generate keys.

Then I created a signature for my barebox boatloder using the cst tool.

I concatenated the signature to the barebox image to create a signed barebox.

When I flash the barebox, I get these HAB events :

I can’t understand what is missing in my signed image ( maybe it is missing a padding)

Can I one who is fimiliar with signing barebox help me to figure out what is missing .

I would really appreciate some help , I have been blocked on this for several days now.

! with The version of barebox that I have barebox can’t sign it self.

I tried configuring the hab configurations

I even tried calling the imx-image script But I didn’t have any luck.

HABv4: Status: Operation failed (0x33)
HABv4: Config: Non-secure IC (0xf0)
HABv4: State: Non-secure state (0x66)
HABv4: -------- HAB Event 0 --------
HABv4: event data:
HABv4: db 00 08 41 33 22 0a 00

HABv4: Status: Operation failed (0x33)
HABv4: Reason: Invalid address: access denied (0x22)
HABv4: Context: Logged in hab_rvt.authenticate_image() (0x0a)
HABv4: Engine: Select first compatible engine (0x00)
HABv4: -------- HAB Event 1 --------
HABv4: event data:
HABv4: db 00 14 41 33 0c a0 00
HABv4: 00 00 00 00 10 00 04 00
HABv4: 00 00 00 20
HABv4: Status: Operation failed (0x33)
HABv4: Reason: Invalid assertion (0x0c)
HABv4: Context: Event logged in hab_rvt.assert() (0xa0)
HABv4: Engine: Select first compatible engine (0x00)
HABv4: -------- HAB Event 2 --------
HABv4: event data:
HABv4: db 00 14 41 33 0c a0 00
HABv4: 00 00 00 00 10 00 04 2c
HABv4: 00 00 03 00
HABv4: Status: Operation failed (0x33)
HABv4: Reason: Invalid assertion (0x0c)
HABv4: Context: Event logged in hab_rvt.assert() (0xa0)
HABv4: Engine: Select first compatible engine (0x00)
HABv4: -------- HAB Event 3 --------
HABv4: event data:
HABv4: db 00 14 41 33 0c a0 00
HABv4: 00 00 00 00 10 00 04 20
HABv4: 00 00 00 01
HABv4: Status: Operation failed (0x33)
HABv4: Reason: Invalid assertion (0x0c)
HABv4: Context: Event logged in hab_rvt.assert() (0xa0)
HABv4: Engine: Select first compatible engine (0x00)
HABv4: -------- HAB Event 4 --------
HABv4: event data:
HABv4: db 00 14 41 33 0c a0 00
HABv4: 00 00 00 00 10 00 10 00
HABv4: 00 00 00 04
HABv4: Status: Operation failed (0x33)
HABv4: Reason: Invalid assertion (0x0c)
HABv4: Context: Event logged in hab_rvt.assert() (0xa0)
HABv4: Engine: Select first compatible engine (0x00)

I used this csf file to sign barebox :

[Header]Version = 4.2Hash Algorithm = sha256Engine Configuration = 0Certificate Format = X509Signature Format = CMSEngine = CAAM

[Install SRK]File = "../crts/SRK_1_2_3_4_table.bin"Source index = 0

[Install CSFK]File = "../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]

[Unlock]Engine = CAAMFeatures = RNG

[Install Key]

Verification index = 0Target index = 2File = "../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate Data]

Verification index = 2Blocks = 0x000 0x000 0x87EE6 "barebox-phytec-phycore-imx6q-som-nand-1gib.img"

0 Kudos
Reply
1 Reply

783 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Maybe someone of  @phytec could help.

 

Regards

0 Kudos
Reply