Hi,
Pls share the i.MX535 Performance Document or Report (either Sabre / EVK) for our benchmarking.
Need to understand the peripheral access speed achieved for Micro-SD/eMMC/USB, etc.
Regards,
Sridevi
Hi Sridevi,
You can go to http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&... to download the IMX53RM. The details of performance and peripheral speed access you can see in it. Hope this can help you ~~
Best Regards
Dan
Thanks Dan for the reply.
My device is based on i.MX535 (Android2.3.7 platform). The design is done almost similar to the i.MX535 based Sabre / QSB.
I need to evaluate the performance of all the interfaces in my device.
For this I would need the practical performance report for the processor interfaces - so i.MX535 based Sabre / QSB performance report would be suitable for the same.
Hope the interface performances would have been evaluated using some tools.
Pls share the relevant document for benchmarking.
Regards,
Sridevi