Request for Links to Files and Instructions for Installing Android OS on IMX6 SABRESDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Links to Files and Instructions for Installing Android OS on IMX6 SABRESDB

460 Views
BDL-DNE
Contributor I

Hello NXP Community,

I’m currently working on loading Android OS onto my IMX6 SABRESDB development board, but I need some help. I’m looking for the direct links to all the required files and a detailed step-by-step guide to get Android up and running on the SABRESDB.

I would really appreciate it if someone could provide the following:

  1. Direct links to the required files:

    • Pre-built Android OS images or the source code.

    • The correct kernel files for the SabresDB board.

    • Any additional dependencies, such as bootloader files or specific device drivers, required for a successful installation.

  2. Step-by-step installation instructions:

    • A complete guide to flashing and installing Android on the DEVELOPMENT BOARD

    • Any configuration steps that need to be followed for optimal functionality.

    • Required tools or utilities (e.g., U-Boot, fastboot, UUU, etc.) to assist with the flashing process.

  3. Troubleshooting Tips (if available):

    • Any common issues that might arise during installation and recommended solutions.

I’ve searched through NXP documentation and forum posts, but I haven’t found a comprehensive guide that covers everything in detail for the SabresDB ,and if android is not available let me know and provide me the same requirements for Linux . Any help, resources, or pointers you can provide would be extremely appreciated!

@android 

@IMX

@IMXSABRESDB

@nxp 

@nxpcommunity 

@nxpcommunity_ 

@Imx6 

@installproblem 

0 Kudos
Reply
5 Replies

406 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can see that in our website the newest android BSP support for the IMX6 SABRESDB is Android P9.0.0_2.2.0 (Linux 4.14.98 kernel),  you can download the documents can refer to.

Rita_Wang_0-1759131941267.png

 

0 Kudos
Reply

213 Views
BDL-DNE
Contributor I
i have been trying with this fles,but facing errors ,can u please help
0 Kudos
Reply

174 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @BDL-DNE 

Of causes I can, What errors you met? Download images or boot error on board?

Best Regards

Rita

0 Kudos
Reply

147 Views
BDL-DNE
Contributor I
This is the error i'm facing

""
ll-7833@LL:~/Documents/IMX6/P9.0.0_2.2/android_p9.0.0_2.2.0-ga_image_6qsabresd $ sudo ./uuu_imx_android_flash.sh -f imx6qp -p sabresd -e
This script is validated with uuu 1.2.135 version, please align with this version.
dtbo is supported
recovery is supported
generate lines to flash u-boot-imx6qp.imx to the partition of bootloader
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx6qp.img to the partition of dtbo
generate lines to flash boot.img to the partition of boot
generate lines to flash recovery-imx6qp.img to the partition of recovery
generate lines to flash system.img to the partition of system
generate lines to flash vendor.img to the partition of vendor
generate lines to flash vbmeta-imx6qp.img to the partition of vbmeta
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.135-0-gacaf035

Success 0 Failure 1 ""

1:11 1/ 1 [HID(W):LIBUSB_ERROR_TIMEOUT ] SDP: boot -f u-boot-imx6qp-sabresd-uuu.imx "
Can you fix this problem or
if it is ok ,can u please suggest me another appropriate Android or Linux Package that i can use insted of the android package that u previously mentioned .
0 Kudos
Reply

74 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi @BDL-DNE ,

You can try to download newest Linux images to the board, it is easy to boot up:

Embedded Linux for i.MX Applications Processors | NXP Semiconductors

Rita_Wang_0-1762066037249.png

For android BSP, when download it need the admin limit.

Android Demo images are here :

Android OS for i.MX Applications Processors | NXP Semiconductors

Any questions contact me freely

Best Regards

Rita

 

 

0 Kudos
Reply