Request for Links to Files and Instructions for Installing Android OS on IMX6 SABRESDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Links to Files and Instructions for Installing Android OS on IMX6 SABRESDB

91 Views
BDL-DNE
Contributor I

Hello NXP Community,

I’m currently working on loading Android OS onto my IMX6 SABRESDB development board, but I need some help. I’m looking for the direct links to all the required files and a detailed step-by-step guide to get Android up and running on the SABRESDB.

I would really appreciate it if someone could provide the following:

  1. Direct links to the required files:

    • Pre-built Android OS images or the source code.

    • The correct kernel files for the SabresDB board.

    • Any additional dependencies, such as bootloader files or specific device drivers, required for a successful installation.

  2. Step-by-step installation instructions:

    • A complete guide to flashing and installing Android on the DEVELOPMENT BOARD

    • Any configuration steps that need to be followed for optimal functionality.

    • Required tools or utilities (e.g., U-Boot, fastboot, UUU, etc.) to assist with the flashing process.

  3. Troubleshooting Tips (if available):

    • Any common issues that might arise during installation and recommended solutions.

I’ve searched through NXP documentation and forum posts, but I haven’t found a comprehensive guide that covers everything in detail for the SabresDB ,and if android is not available let me know and provide me the same requirements for Linux . Any help, resources, or pointers you can provide would be extremely appreciated!

@android 

@IMX

@IMXSABRESDB

@nxp 

@nxpcommunity 

@nxpcommunity_ 

@Imx6 

@installproblem 

0 Kudos
Reply
1 Reply

37 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can see that in our website the newest android BSP support for the IMX6 SABRESDB is Android P9.0.0_2.2.0 (Linux 4.14.98 kernel),  you can download the documents can refer to.

Rita_Wang_0-1759131941267.png

 

0 Kudos
Reply