Request for LPDDR4 byte swapping in i.MX8DXL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Request for LPDDR4 byte swapping in i.MX8DXL

1,290 次查看
puneethkumar
Contributor III

Dear Team,

In the hardware guide of i.MX8DXL it is mentioned like Byte swapping within the 16-bit channel is not supported in case of i.MX8DXL.

1) What does it mean exactly.

2) In the reference schematics they have done bitswapping with one one byte - is that ok? 

0 项奖励
回复
1 回复

1,286 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Puneeth

 

1. In case of 8DXL/SXL, byte swapping is not allowed with LPDDR4 but is allowed with DDR3L.
This is due to SoC design limitation, which would prevent to correctly read the mode registers if

the data bytes were swapped. Then, since DDR3L does not support mode register reads, the byte swapping restriction does not apply to it.

 

2. it is ok

 

Best regards
igor

 

 

0 项奖励
回复