Hello, igor
we check the uboot .config , the OPTEE is not set
we test on the 4.14.98-2.2.0 release , only change the PHYS_SDRAM_SIZE to 4G :#define PHYS_SDRAM_SIZE 0x100000000,
it is fail also , when update the firmware by uuu.exe.
Hello, igor
There is another question need your help.
the params of the Number of ROW Addresses is 16 or 17, which is inputed ?
as the below 32G be used (32gb, R[16:0],c[9:0]),
 
Beset Regards
feng
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi feng
issue may be related to TEE, one can disable it using sect.5.6.11 OP-TEE
attached Yocto Guide.
TEE can't be set in the top of the memory if 4GB are used, because above 4GB space,
only A53 can use it, So for i.MX8MQ one can split 4GB memory as 3GB + 1GB and keep
TZ address not changed. Also recommended to use release L4.14.98_2.1.0 and later, which
has 4 GB support implemented by default. 
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------