The Low-Resolution Analog-Digital Converter is a multipurpose module used to measure the voltage applied to dedicated input pins. Some of the input pins can be used to interface a resistive touchscreen, while other pins can be used for general purpose inputs such as keypad. The LRADC controller is not used directly by the software.
However if you would like to disable the keypad on the evaluation board as some of the pins are used for other functions in the EVK, the environment variable BSP_NOKEYPAD is defined to exclude the keypad. We then follow the reference manual to include the following item,
Third Party > BSP > Freescale i.MX28 EVK: PDK1_9:ARMV4I > Device Drivers > KEYPAD> KEYPAD
Hope it helps