Relationship between waveform disturbance and operation problem in MIPI HS mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Relationship between waveform disturbance and operation problem in MIPI HS mode

Jump to solution
1,025 Views
Takuya-k
Contributor II

 

Hello.

I am trying to send an image from MCIMX8M-EVK to the original DSI panel with MIPI-DSI, but it does not work.
It worked a few times, but when I restart the EVK after it works, it doesn't work.
Most likely it won't work.
The only change in the state before and after restarting is connecting and disconnecting the connection cable.
(The state expressed as working is the state in which the number of received image frames on the panel side is increasing.)

The waveform of the HS mode data line is attached.
When the left side moves, when the right side does not move.

Is there a possibility that the register setting is bad as the cause of the above not working?

The DSI panel cannot receive data just by restarting the EVK, and the HS mode waveform is distorted. I don't know the reason for this.

Regarding EMI (mixture of noise), I think it is different because there is no noise in the LP mode waveform.

best regards.

Takuya.

0 Kudos
Reply
1 Solution
1,010 Views
Takuya-k
Contributor II

Hi Sir,
Withdraw the question.

Regards.
Takuya.

View solution in original post

0 Kudos
Reply
1 Reply
1,011 Views
Takuya-k
Contributor II

Hi Sir,
Withdraw the question.

Regards.
Takuya.

0 Kudos
Reply