[Regression] X crash on Yocto startup with BSP 3.5.7-1.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[Regression] X crash on Yocto startup with BSP 3.5.7-1.0.0

2,960 次查看
DiegoFSL
Contributor III

Hi i.MX community,

I'd like to advise that although with latest BSP 3.5.7-1.0.0 Yocto has gained support for hardfloat, it "somehow" lost support for softfloat.

It's not that's really lost; but there's a severe regression in X support: there's an X crash on startup (which does not happen on hardfloat variant).

Here's full Xorg.0.log:

http://pastebin.com/U8TEcZiA

Did anybody else test X11 on a Yocto BSP 3.5.7-1.0.0 softfloat build?

Bye,

Diego

标签 (4)
0 项奖励
回复
7 回复数

2,042 次查看
OtavioSalvador
Senior Contributor II

This has been fixed in master branch of Yocto BSP and will be available in 1.5 release.

0 项奖励
回复

2,042 次查看
EricNelson
Senior Contributor II

Hi Diego,

How are you disabling hard-float?

It appears that the DEFAULTTUNE settings are un-conditional:

~/yocto-3.5.7/sources$ for f in meta-fsl-* ; do grep -r DEFAULTTUNE $f/* ; done
meta-fsl-bsp-release/imx/README:DEFAULTTUNE_mx6 = "cortexa9hf-neon
meta-fsl-bsp-release/imx/meta-fsl-arm/conf/machine/include/fsl-mx6-common.inc:DEFAULTTUNE_mx6 = "cortexa9hf-neon"
meta-fsl-bsp-release/imx/meta-fsl-arm/conf/layer.conf:DEFAULTTUNE_mx6 = "cortexa9hf-neon"

I think those DEFAULTTUNE_mx6 = "cortexa9hf-neon" statements should use ?=.

0 项奖励
回复

2,042 次查看
DiegoFSL
Contributor III

Hi Eric,

I think you're using meta-fsl-* from Freescale, but I suggest you to use traditional Yocto ones, and switch to master-next for meta-fsl-arm, meta-fsl-arm-extra and meta-fsl-demos.

Then you'll have:

$ for f in meta-fsl-* ; do grep -r DEFAULTTUNE $f/* ; done
meta-fsl-arm/conf/machine/include/imx-base.inc:DEFAULTTUNE_mx6 ?= "cortexa9hf-neon"

Then setting DEFAULTTUNE in local.conf should work:

http://git.yoctoproject.org/cgit/cgit.cgi/meta-fsl-arm/commit/?h=master-next&id=970a07a4d56b521cfffe...

Bests,

Diego

0 项奖励
回复

2,042 次查看
EricNelson
Senior Contributor II

Thanks Diego,

You're absolutely right, and I'll try the Yocto versions.

0 项奖励
回复

2,042 次查看
LeonardoSandova
Specialist I

Diego,

which image/machine are you building?

(FYI LaurenPost / EnriqueOchoaVazquez)

0 项奖励
回复

2,042 次查看
DiegoFSL
Contributor III

I'm building fsl-image-gui for machine Nitrogen6x.

See also bug report:

https://bugzilla.yoctoproject.org/show_bug.cgi?id=4946

0 项奖励
回复

2,042 次查看
LaurenPost
NXP Employee
NXP Employee

I tried this on imx6qsabresd and have no issues.   Right before release we did have problems with disabling hwfp correctly but it was enabled in the final update.

Also I've seen multiple times that switching between hwfp and swfp can corrupt build states.  I always keep these completely separate builds both with cache and tmp directories.  

0 项奖励
回复