Regarding the RMII interface on i.MX8M nano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding the RMII interface on i.MX8M nano

Jump to solution
823 Views
yan_ding
Contributor I

Hello,

We are developing a hardware system based on i.mx8m nano. I have a question on the RGMII/RMII interface. According to "i.MX 8M Nano Applications Processor Datasheet for Industrial Products":

On page 42:

"For RMII—ENET_TD2 functions as RMII REF_CLK when configured in the ALT1 mode."

On page 43:

"For RMII—SD1_RESET_B functions as RMII REF_CLK when configured in the ALT1 mode."

I wonder in the ALT0 mode which is the REF_CLK signal? Or is there something wrong with this datasheet?


Thanks!

Labels (1)
0 Kudos
1 Solution
803 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

There is nothing wrong with the datasheet. It is just that for getting the REF_CLK through either pad you mentioned, it is required to use the ALT1; for ALT0 this would not be possible.

Hope it helps!

 

BR,

Ivan.

View solution in original post

0 Kudos
2 Replies
804 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

There is nothing wrong with the datasheet. It is just that for getting the REF_CLK through either pad you mentioned, it is required to use the ALT1; for ALT0 this would not be possible.

Hope it helps!

 

BR,

Ivan.

0 Kudos
792 Views
yan_ding
Contributor I

Thank you Ivan.

0 Kudos