Regarding kpp.c for imxrt1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding kpp.c for imxrt1050

1,416 Views
PriyaMP
Contributor I

Hi All,

We are testing kpp.c sdk driver in our custom board.

But the sdk example doesn't seem to work.

PFA for the screenshots of the design.

Kindly help us wrt this asap.

Labels (1)
Tags (1)
0 Kudos
2 Replies

1,389 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello PriyaMP,

The following thread may be of help. Additionally, if you are using the SDK example I would double check that the pin configuration is updated to that of your custom board.

https://community.nxp.com/t5/i-MX-RT/Keypad-Port-KPP-on-the-i-MX-RT1010-EVK/m-p/1021498

I hope that this information helps!

Regards,
Gustavo

0 Kudos

1,381 Views
PriyaMP
Contributor I

Hi gusarambula,

Thank you for the response.

Our custom board has 3x2 Matrix Keypad

ROW1 : H12
ROW2 : L13
ROW3 : H13
COL1 : H11
COL2 : J13

I've updated the kpp sdk according to our custom board.

PFA for the project and custom board pin details.

Can you please confirm if I've updated according to my custom board?

Kindly help us asap.

Thank you.

0 Kudos