Hello PriyaMP,
The following thread may be of help. Additionally, if you are using the SDK example I would double check that the pin configuration is updated to that of your custom board.
https://community.nxp.com/t5/i-MX-RT/Keypad-Port-KPP-on-the-i-MX-RT1010-EVK/m-p/1021498
I hope that this information helps!
Regards,
Gustavo
Hi gusarambula,
Thank you for the response.
Our custom board has 3x2 Matrix Keypad
ROW1 : H12
ROW2 : L13
ROW3 : H13
COL1 : H11
COL2 : J13
I've updated the kpp sdk according to our custom board.
PFA for the project and custom board pin details.
Can you please confirm if I've updated according to my custom board?
Kindly help us asap.
Thank you.