Regarding guard band output in HDMI/DVI output mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding guard band output in HDMI/DVI output mode.

2,492 Views
Yoshiharaaa
Contributor I

In the HDMI certification test, the ID7-33 HDMI/DVI output mode compatibility test result was FAIL.

Questions
・Guard band was not transmitted in all five tests of ID:7-33.
Isn't the guard band itself not being transmitted as a function?
(Contradiction: In the test results for ID:7-33a using the same software, a guard band is transmitted.)
・I initialize before switching to HDMI/DVI mode, but is there any logic to allow/disallow guard band transmission?
・Is VSDB involved in permitting/disallowing guard band transmission?

Yoshiharaaa_0-1699922691473.png

Please let me know how to solve this problem.

Thank you.
Yoshihara

0 Kudos
Reply
7 Replies

2,474 Views
joanxie
NXP TechSupport
NXP TechSupport

which HDMI of processor do you use?

0 Kudos
Reply

2,468 Views
Yoshiharaaa
Contributor I

Thank you for reply.

I used a device with IMX8MP and took the certification test for HDMI 1.4b Source device.

I would like to know why the guard band is not output when outputting HDMI and how to control it.

Thank you.

 

@joanxie 

0 Kudos
Reply

2,349 Views
joanxie
NXP TechSupport
NXP TechSupport

did you test on the latest bsp version?

0 Kudos
Reply

2,329 Views
Yoshiharaaa
Contributor I

Hello,@joanxie san

Sorry, I will make some corrections as a result of the investigation.
We have confirmed that the reason why Guard Band is not output is that the HDMI/DVI mode switching is not done properly.If the mode switching is done, it will work normally.

When reading EDID, the HDMI/DVI mode cannot be switched properly, and the previous information appears to be reflected.
Even if you reset the HDP, the mode does not change at all, and it will be reflected when the power is turned on again.
application, but HDMI/DVI does not switch properly.
I would like to know the solution.

Test ItemResult
No.EDID(Expected value)Pattern1Pattern2
1DVIDVIHDMI
2HDMIDVIDVI
3HDMIDVIHDMI
4DVIDVIHDMI
5HDMIDVIDVI
Process 1 to 5 in order  

 

>did you test on the latest bsp version?

 The kernel will be v5.4.24-2.1.0.
 The version of yocto is 3.0.2.

 

Thank you,

yoshihara

0 Kudos
Reply

2,300 Views
joanxie
NXP TechSupport
NXP TechSupport

did you pass 7-1 test? which is related to the  EDID IF

0 Kudos
Reply

2,210 Views
Yoshiharaaa
Contributor I

@joanxie -san

 

Sorry for the delay in my reply.
I passed ID:7-1.

I researched this issue and was able to resolve it the other day.
The reason for not being able to switch HDMI/DVI after obtaining EDID was in the user application.

I successfully passed the HDMI compliance test.

Thank you for your support.

 

Thank you,

Yoshihara

0 Kudos
Reply

2,204 Views
joanxie
NXP TechSupport
NXP TechSupport

glad to hear this and share this useful information here

0 Kudos
Reply