Hi,
Can you please let me know the maximum frequency of operation for SCLK of LPSPI Master mode of MIMXRT1176CVM8A (MIMXRT1176 family).
As per the datasheet, (Document Number: IMXRT1170IEC Rev. 4, 05/2023)
1) Max value of fSCK is given as fperiph/2. (Page 88 of datasheet)
But i could not get the value of fperiph.
2) Also, there is a note for fSCK in page 88 that says "Absolute maximum frequency of operation (fop) is 30 MHz. The clock driver in the LPSPI module for fperiph must guaranteed this limit is not exceeded".
Can you please look into these two points and tell me the max fSCK for LPSPI master mode.