Regarding connection between SSI and AUDMUX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding connection between SSI and AUDMUX

1,780 次查看
yuji_fuseki
Contributor II

Hi, 

Please let me make clear about below questions.

 1) Each SSIx(x=1,2,3) is included STCK/STFS/SRCK/SRFS/STXD/SRXD signal lines?

 2) Each SSIx(x=1,2,3) are connected to internal port 1/2/7 of AUDMUX. Is this understanding correct?

 3) we can set port to port connection inside AUDMUX?(default configuration is below figure)

 pastedImage_8.png

 Best regards,

yuji

0 项奖励
回复
4 回复数

1,689 次查看
yuji_fuseki
Contributor II

Dear Igor, 

Please let me ask an additional question about relationship of signal name for each module; SSI, AUDMUX and  IOMUX.

Below relationship about signal name is correct?

[SSI]                              [AUDMUX(x=3,4,5,6)]                              [IOMUX(x=3,4,5,6)]

1.STCK     <--------->     TxCLKx                            <--------->          AUDx_TXC

2.STFS     <--------->      TxFSx                              <--------->          AUDx_TXFS

3.STXD     <--------->     TxDx                                <--------->          AUDx_TXD

4.SRCK     <--------->     RxCLKx                           <--------->          AUDx_RXC

 (network clk)

5.SRFS     <--------->     RxFSx                             <--------->          AUDx_RXFS

6.SRXD     <--------->    RxDx                               <--------->          AUDx_RXD

 

Br,

Yuji

0 项奖励
回复

1,689 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuji

interconnections are described in AN2628

https://www.nxp.com/docs/en/application-note/AN2628.pdf 

Best regards
igor

0 项奖励
回复

1,689 次查看
yuji_fuseki
Contributor II

Hi, Igor

thanks for you explanation.

I understood.

Br,

yuji

0 项奖励
回复

1,689 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuji

1. yes

2. this depends on used processor, for example for i.MX6Q it is described in

Table 81. AUDMUX Port Allocation

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

3. right

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复