Regarding DDR3 for iMX6 Quad

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Regarding DDR3 for iMX6 Quad

ソリューションへジャンプ
1,517件の閲覧回数
SreedharNair
Contributor I

Hi Guys,

I have few more doubts regarding ddr3 for imx6,

1, Is it possible to design the imx6 with only one ddr3 chip (512 MB) ? The imx6 design guide shows 2 Gbyte and 4 Gbyte configurations which has 4 and 8 chips respectively. If we can design with one chip then does it mean the layout is in flyby topology and we need to include termination resistors?

2, Is there any difference between layout requirements for ddr3 and ddr3L other than the voltage requirement for imx6 ?

Regards,
Sreedhar

ラベル(1)
0 件の賞賛
返信
1 解決策
1,510件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SreedharNair

 

1.> Is it possible to design the imx6 with only one ddr3 chip (512 MB) ?

 

yes

 

> If we can design with one chip then does it mean the layout is in flyby

>topology and we need to include termination resistors?

 

no need for flyby and termination.

 

2. no differencies

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,511件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SreedharNair

 

1.> Is it possible to design the imx6 with only one ddr3 chip (512 MB) ?

 

yes

 

> If we can design with one chip then does it mean the layout is in flyby

>topology and we need to include termination resistors?

 

no need for flyby and termination.

 

2. no differencies

 

Best regards
igor

0 件の賞賛
返信
1,505件の閲覧回数
SreedharNair
Contributor I

@igorpadykov  Thanks so much for your reply.

I have one more query if we are using byte group 1 and 2 for the single memory chip, What is to be done with the remaining byte group pads? Do we leave then not connected or do we have to ground then?

Thanks in Advance,

Sreedhar

 

0 件の賞賛
返信
1,500件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi SreedharNair

 

they can be left unconnected.

 

Best regards
igor

0 件の賞賛
返信