Regarding DDR3 for iMX6 Quad

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding DDR3 for iMX6 Quad

Jump to solution
856 Views
SreedharNair
Contributor I

Hi Guys,

I have few more doubts regarding ddr3 for imx6,

1, Is it possible to design the imx6 with only one ddr3 chip (512 MB) ? The imx6 design guide shows 2 Gbyte and 4 Gbyte configurations which has 4 and 8 chips respectively. If we can design with one chip then does it mean the layout is in flyby topology and we need to include termination resistors?

2, Is there any difference between layout requirements for ddr3 and ddr3L other than the voltage requirement for imx6 ?

Regards,
Sreedhar

Labels (1)
0 Kudos
Reply
1 Solution
849 Views
igorpadykov
NXP Employee
NXP Employee

Hi SreedharNair

 

1.> Is it possible to design the imx6 with only one ddr3 chip (512 MB) ?

 

yes

 

> If we can design with one chip then does it mean the layout is in flyby

>topology and we need to include termination resistors?

 

no need for flyby and termination.

 

2. no differencies

 

Best regards
igor

View solution in original post

0 Kudos
Reply
3 Replies
850 Views
igorpadykov
NXP Employee
NXP Employee

Hi SreedharNair

 

1.> Is it possible to design the imx6 with only one ddr3 chip (512 MB) ?

 

yes

 

> If we can design with one chip then does it mean the layout is in flyby

>topology and we need to include termination resistors?

 

no need for flyby and termination.

 

2. no differencies

 

Best regards
igor

0 Kudos
Reply
844 Views
SreedharNair
Contributor I

@igorpadykov  Thanks so much for your reply.

I have one more query if we are using byte group 1 and 2 for the single memory chip, What is to be done with the remaining byte group pads? Do we leave then not connected or do we have to ground then?

Thanks in Advance,

Sreedhar

 

0 Kudos
Reply
839 Views
igorpadykov
NXP Employee
NXP Employee

Hi SreedharNair

 

they can be left unconnected.

 

Best regards
igor

0 Kudos
Reply