Regarding 1080p decoding in imx6 sabre AI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding 1080p decoding in imx6 sabre AI

783 Views
srilakshmikanag
Contributor I

Hi,

At present I am working on sabre platform for autoinfotainment.

Can "i.MX6 Quad" supports DUAL instance 1080p h264 decoding?

Please let me know

Regards,

Srilakshmi

0 Kudos
2 Replies

492 Views
4guin4g4
Contributor IV

Yes, it can perform 2 full HDS @ 30fps  decode or encode.

0 Kudos

492 Views
FranciscoCarril
Contributor V

2 Full HD decode is possible   if     videos are @24 fps.  When VPU is used at 266mhz which is the common situation

This is due to VPU troughput characteristics.

If VPU is set at 352MHZ  it can handle @30fps, but this feature is still under test.

0 Kudos