Logitech USB webcam connected to imx6q board is getting connected. But if I launch any of the application to test webcam, the port resets and the webcam is getting disconnected. Please help me on this. Below is the error I'm getting
#fswebcam
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
hub 1-0:1.0: Cannot enable port 1. Maybe the USB cable is bad?
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
ci_hdrc ci_hdrc.0: port 1 reset error -110
But the same webcam is working fine in PC. ANd also when I connect USB keyboard/mouse to board there is no error.
Hi shalini
first try to verify if this camera is uvc camera.
Also it may be necessary to modprobe driver for camera before usage:
Using a USB Camera with GStreamer
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks for d reply. It is a UVC camera. Camera driver is added. can see "dev/video0". The problem is the port is getting reset and webcam is getting disconnected.
one can try with Demo image :
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)