Redundant boot build Instructions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Redundant boot build Instructions

2,181 Views
lockit282
Contributor III

1. Is there documentation for building the redundant bootloader (secondary boot) without fastboot for the imx8mm in an android environment?
2. Can the Secondary bootloader be used in a non-secure environment -- manually set the PErsist bit)?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,869 Views
lockit282
Contributor III

My question is -- what is the best way to get the secondary image table onto the emmc per the documentation in the imx8mm security manual -- and this app note : i.MX 8MQ - ROM Redundant Boot for expansion device 
1. When I look at the fastboot code to flash u-boot the start offset on the emmc is 0x42

2. I am using an Android environment w/Secure boot

Question 1: How to program the secondary image table on the imx8mm eMMC per Chapter 6 of the Imx8mm Security manual?

Question 2: The secondary bootloader -- can it be a copy of the primary?

0 Kudos
Reply

1,869 Views
lockit282
Contributor III

This for flashing onto emmc

0 Kudos
Reply