Recovery time from SUSPEND and WAIt modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recovery time from SUSPEND and WAIt modes

913件の閲覧回数
MarkoPanger
Contributor III

The i.MX5x PM driver supports different modes of low power operations.

I'm particularly interested in the:

- STOP mode which maps to "Suspend to RAM"

- WAIT mode which maps to "Standby" mode

Does anybody know what is the recovery time needed from the low poer modes listed above to full running mode ?

Our idea is to read an ADC value each 1s. If the value is below a certain threshold we get back to WAIT (or STOP mode depending of the staus of the external PSU) mode. Are such fast (1 second) transition times even possible ? Looking at the source there should be no limitations, except for some PLL setup times.

Any thoughts, comments ?

Marko

タグ(1)
0 件の賞賛
返信
0 返答(返信)