Recommended topology when 2 chips DDR3 are connected to i.MX6.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Recommended topology when 2 chips DDR3 are connected to i.MX6.

跳至解决方案
2,399 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6 series DDR3 connection.

They want to know the recommended topology when two chips DDR3 are connected to i.MX6.

In this case, should they use fly-by topology? or T-branch topology?

I feel fly-by topology is better because write leveling can use to it, but could you let me know Freescale recommendation?

Best Regards,

Satoshi Shimoda

标签 (6)
标记 (1)
0 项奖励
回复
1 解答
1,694 次查看
aven_tsao
NXP Employee
NXP Employee

Hi Satoshi:

Both T-topo and Fly-By design are ok in 2 ddr chips case.

But we suggest use T-topology design in 4 (and 2) ddr chips case, because the Fly-by design need additional power supply for external termination resistors.

(It will increase the cost and power consumption).

Please reference to the section 3.5 Routing considerations in MX6 HDG for the detail.

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf?fasp=1&WT_TYPE=Users Guides&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation&fileExt=.pdf

Best regards

Aven

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,695 次查看
aven_tsao
NXP Employee
NXP Employee

Hi Satoshi:

Both T-topo and Fly-By design are ok in 2 ddr chips case.

But we suggest use T-topology design in 4 (and 2) ddr chips case, because the Fly-by design need additional power supply for external termination resistors.

(It will increase the cost and power consumption).

Please reference to the section 3.5 Routing considerations in MX6 HDG for the detail.

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf?fasp=1&WT_TYPE=Users Guides&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation&fileExt=.pdf

Best regards

Aven

0 项奖励
回复