Should the WRITE_LEVELING delay register values be set greater than the worst case delay value measured across boards?
The documents and discussions usually defer to using a model of the design to set the WRITE_LEVELING delay, but from our measurements using the DDR Stress Test, there is significant deviation board to board which may not align with a modeled design center. Proposing to set delays in the shape of the average line but offset to where they are beyond the worst case delays
解決済! 解決策の投稿を見る。
Hi jschoen
I am afraid it is not true to use worst case delay value measured
across boards. Ideally board should use own WRITE_LEVELING delay register values.
Difference accross boards may be caused by impedance mismatch or board noise.
One can recheck with sect.3.4 DDR routing rules IMX6DQ6SDLHDG
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Igor,
I found this related post : https://community.freescale.com/thread/319387
It suggests sampling 5-10 boards and get calibration values. Then balance the write leveling values (normally average them). This is essentially what we've done....obtained calibration values for a sample build of same board design.
Is it recommended to average the write leveling value or use the worst case delay value?
Thanks.
Joel
Hi jschoen
procedure normally to average them
Best regards
igor