Reboot failed -- System halted(imx6q)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reboot failed -- System halted(imx6q)

9,199 次查看
1042484520
Contributor II

Dear NXP:

[ 18.684772] reboot: Restarting system
[ 18.688457] CPU: 0 PID: 440 Comm: reboot Not tainted 4.9.11-1.0.0+gc27010d99a3d #6
[ 18.696032] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 18.702597] [<8010f954>] (unwind_backtrace) from [<8010b398>] (show_stack+0x10/0x14)
[ 18.710359] [<8010b398>] (show_stack) from [<803c0918>] (dump_stack+0x78/0x8c)
[ 18.717597] [<803c0918>] (dump_stack) from [<80109ac0>] (machine_restart+0xc/0x80)
[ 18.725181] [<80109ac0>] (machine_restart) from [<8014c640>] (SyS_reboot+0xc8/0x1ac)
[ 18.732937] [<8014c640>] (SyS_reboot) from [<80107880>] (ret_fast_syscall+0x0/0x3c)
[ 18.840659] imx2-wdt 20c0000.wdog: failed to assert external reset, trying with timeout
[ 19.848669] Reboot failed -- System halted

标签 (1)
0 项奖励
回复
3 回复数

8,585 次查看
DiegoFSL
Contributor III

If you don't have PMIC you can't use the external reset.

In this case keep wdog1 enabled and wdog2 disabled, which is the default configuration for imx6qdl.dtsi:

imx6qdl.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

This is overriden in SABRE SD EVK dts:

imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel

so you need to make sure wdog1 and wdog2 configuration from imx6qdl.dtsi is not overridden somewhere in your board dts hierarchy.

0 项奖励
回复

8,586 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello qingzong,

Try removing the pfuze100 from the kernel, and see that it can be boot up

Regards

0 项奖励
回复

8,586 次查看
1042484520
Contributor II

Hi Bio:

      Still can't restart after removal.

Thx!

0 项奖励
回复