Real-time Edge for i.MX8QM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Real-time Edge for i.MX8QM?

759 Views
lorenzo_giraudi
Contributor III

Hello,

I have just discovered the Real-time Edge framework for Layerscape and imx8mm. Is there something useful that can be used also on i.mx8QM? What are the differences?

Thanks

0 Kudos
Reply
2 Replies

752 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello lorenzo,

 

The MX8QM has hypervisor Level 2, and can not run jailhouse for PREEMP_RT, so it is not supported.

 

Regards

0 Kudos
Reply

418 Views
ente59
Contributor I

Hello, not knowing what "hypervisor Level 2" is i details, but we're using i.mx8QM and are thinking about to use "Real-time Edge framework" too.

Is there a plan "Real-time Edge framework" will support i.mx8QM next time?

Kind regards

Heiko

0 Kudos
Reply