Reading data from an FPGA connected to the iMX6q EIM bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading data from an FPGA connected to the iMX6q EIM bus

2,966件の閲覧回数
shanql
Contributor I

我需要使用MCIMX6Q6AVT10AC 的EIM接口读取FPGA,

我把imx6q的EIM_DA0----EIM_DA13作为RAM地址线,EIM_D16---EIM_D31作为RAM的数据线。使用了EIM_RW  EIM_OE  EIM_CS0 

EIM_WAIT  EIM_EB0  EIM_EB1,与FPGA相连

我按照board-mx6q_sabreauto.h和board-mx6q_sabreauto.c中的weimnor例子做了如下改动:

====================================================================================

1,

我在linux内核,在board-mx6q_sabresd.h中增加了

static iomux_v3_cfg_t mx6q_weimnor_pads[] __initdata = {

  /* Parallel NOR */

  MX6Q_PAD_EIM_OE__WEIM_WEIM_OE,

  MX6Q_PAD_EIM_RW__WEIM_WEIM_RW,

  MX6Q_PAD_EIM_WAIT__WEIM_WEIM_WAIT,

  MX6Q_PAD_EIM_CS0__WEIM_WEIM_CS_0,

  MX6Q_PAD_EIM_CS1__WEIM_WEIM_CS_1,

  /*Control NOR reset using gpio mode*/

  //MX6Q_PAD_DISP0_DAT8__GPIO_4_29,

  MX6Q_PAD_EIM_LBA__WEIM_WEIM_LBA,

  MX6Q_PAD_EIM_BCLK__WEIM_WEIM_BCLK,

  /* Parallel Nor Data Bus */

  MX6Q_PAD_EIM_D16__WEIM_WEIM_D_16,

  MX6Q_PAD_EIM_D17__WEIM_WEIM_D_17,

  MX6Q_PAD_EIM_D18__WEIM_WEIM_D_18,

  MX6Q_PAD_EIM_D19__WEIM_WEIM_D_19,

  MX6Q_PAD_EIM_D20__WEIM_WEIM_D_20,

  MX6Q_PAD_EIM_D21__WEIM_WEIM_D_21,

  MX6Q_PAD_EIM_D22__WEIM_WEIM_D_22,

  MX6Q_PAD_EIM_D23__WEIM_WEIM_D_23,

  MX6Q_PAD_EIM_D24__WEIM_WEIM_D_24,

  MX6Q_PAD_EIM_D25__WEIM_WEIM_D_25,

  MX6Q_PAD_EIM_D26__WEIM_WEIM_D_26,

  MX6Q_PAD_EIM_D27__WEIM_WEIM_D_27,

  MX6Q_PAD_EIM_D28__WEIM_WEIM_D_28,

  MX6Q_PAD_EIM_D29__WEIM_WEIM_D_29,

  MX6Q_PAD_EIM_D30__WEIM_WEIM_D_30,

  MX6Q_PAD_EIM_D31__WEIM_WEIM_D_31,

  /* Parallel Nor 25 bit Address Bus */

  MX6Q_PAD_EIM_A24__GPIO_5_4,

  MX6Q_PAD_EIM_A23__WEIM_WEIM_A_23,

  MX6Q_PAD_EIM_A22__WEIM_WEIM_A_22,

  MX6Q_PAD_EIM_A21__WEIM_WEIM_A_21,

  MX6Q_PAD_EIM_A20__WEIM_WEIM_A_20,

  MX6Q_PAD_EIM_A19__WEIM_WEIM_A_19,

  MX6Q_PAD_EIM_A18__WEIM_WEIM_A_18,

  MX6Q_PAD_EIM_A17__WEIM_WEIM_A_17,

  MX6Q_PAD_EIM_A16__WEIM_WEIM_A_16,

  MX6Q_PAD_EIM_DA15__WEIM_WEIM_DA_A_15,

  MX6Q_PAD_EIM_DA14__WEIM_WEIM_DA_A_14,

  MX6Q_PAD_EIM_DA13__WEIM_WEIM_DA_A_13,

  MX6Q_PAD_EIM_DA12__WEIM_WEIM_DA_A_12,

  MX6Q_PAD_EIM_DA11__WEIM_WEIM_DA_A_11,

  MX6Q_PAD_EIM_DA10__WEIM_WEIM_DA_A_10,

  MX6Q_PAD_EIM_DA9__WEIM_WEIM_DA_A_9,

  MX6Q_PAD_EIM_DA8__WEIM_WEIM_DA_A_8,

  MX6Q_PAD_EIM_DA7__WEIM_WEIM_DA_A_7,

  MX6Q_PAD_EIM_DA6__WEIM_WEIM_DA_A_6,

  MX6Q_PAD_EIM_DA5__WEIM_WEIM_DA_A_5,

  MX6Q_PAD_EIM_DA4__WEIM_WEIM_DA_A_4,

  MX6Q_PAD_EIM_DA3__WEIM_WEIM_DA_A_3,

  MX6Q_PAD_EIM_DA2__WEIM_WEIM_DA_A_2,

  MX6Q_PAD_EIM_DA1__WEIM_WEIM_DA_A_1,

  MX6Q_PAD_EIM_DA0__WEIM_WEIM_DA_A_0,

};

====================================================================================

2,在board-mx6q_sabresd.c中增加了

static struct mtd_partition mxc_nor_partitions[] = {

  {

  .name = "bootloader",

  .offset = 0,

  .size = SZ_256K,

  }, {

  .name = "bootenv",

  .offset = MTDPART_OFS_APPEND,

  .size = SZ_256K,

  .mask_flags = MTD_WRITEABLE,

  }, {

  .name = "kernel",

  .offset = MTDPART_OFS_APPEND,

  .size = SZ_4M,

  }, {

  .name = "rootfs",

  .offset = MTDPART_OFS_APPEND,

  .size = MTDPART_SIZ_FULL,

  },

};

static struct resource nor_flash_resource = {

  .start = CS0_BASE_ADDR,

  .end = CS0_BASE_ADDR  +  0x02000000 - 1,

  .flags = IORESOURCE_MEM,

};

static struct physmap_flash_data nor_flash_data = {

  .probe_type = "map_rom",

  .width = 2,

  .parts = mxc_nor_partitions,

  .nr_parts = ARRAY_SIZE(mxc_nor_partitions),

};

static struct platform_device physmap_flash_device = {

  .name = "physmap-flash",

  .id = 0,

  .dev = {

  .platform_data = &nor_flash_data,

  },

  .resource = &nor_flash_resource,

  .num_resources = 1,

};

/* These registers settings are just valid for Numonyx M29W256GL7AN6E. */

static void mx6q_setup_weimcs(void)

{

  void __iomem *nor_reg = MX6_IO_ADDRESS(WEIM_BASE_ADDR);

  void __iomem *ccm_reg = MX6_IO_ADDRESS(CCM_BASE_ADDR);

  unsigned int reg;

  struct clk *clk;

  u32 rate;

  /* CLKCTL_CCGR6: Set emi_slow_clock to be on in all modes */

  reg = readl(ccm_reg + 0x80);

  reg |= 0x00000C00;

  writel(reg, ccm_reg + 0x80);

  /* Timing settings below based upon datasheet for M29W256GL7AN6E

    These setting assume that the EIM_SLOW_CLOCK is set to 132 MHz */

  clk = clk_get(NULL, "emi_slow_clk");

  if (IS_ERR(clk))

  printk(KERN_ERR "emi_slow_clk not found\n");

  rate = clk_get_rate(clk);

  if (rate != 132000000)

  printk(KERN_ERR "Warning: emi_slow_clk not set to 132 MHz!"

        " WEIM NOR timing may be incorrect!\n");

  /*

  * For EIM General Configuration registers.

  *

  * CS0GCR1:

  * GBC = 0; CSREC = 6; DSZ = 2; BL = 0;

  * CREP = 1; CSEN = 1;

  *

  * EIM Operation Mode: MUM = SRD = SWR = 0.

  * (Async write/Async page read, none multiplexed)

  *

  * CS0GCR2:

  * ADH = 1

  */

  writel(0x00626481, nor_reg);//writel(0x00620081, nor_reg);

  writel(0x00000001, nor_reg + 0x00000004);

  /*

  * For EIM Read Configuration registers.

  *

  * CS0RCR1:

  * RWSC = 1C;

  * RADVA = 0; RADVN = 2;

  * OEA = 2; OEN = 0;

  * RCSA = 0; RCSN = 0

  *

  * CS0RCR2:

  * APR = 1 (Async Page Read);

  * PAT = 4 (6 EIM clock sycles)

  */

  //writel(0x1C022000, nor_reg + 0x00000008);

  //writel(0x0000C000, nor_reg + 0x0000000C);

  writel(0x0b010000, nor_reg + 0x00000008);

  writel(0x00000008, nor_reg + 0x0000000C);

  /*

  * For EIM Write Configuration registers.

  *

  * CS0WCR1:

  * WWSC = 20;

  * WADVA = 0; WADVN = 1;

  * WBEA = 1; WBEN = 2;

  * WEA = 1; WEN = 6;

  * WCSA = 1; WCSN = 2;

  *

  * CS0WCR2:

  * WBCDD = 0

  */

  //writel(0x1404a38e, nor_reg + 0x00000010);

  writel(0x0b040040, nor_reg + 0x00000010);

  writel(0x00000000, nor_reg + 0x00000014);

}

====================================================================================

3,在board-mx6q_sabresd.c中的函数mx6_sabresd_board_init(void)增加了

  mx6q_setup_weimcs();

  platform_device_register(&physmap_flash_device);

======================================================================================

现在我想通过IMX6Q的EIM接口访问RAM(fpga),以上的设置是否正确,还有EIM_CS0GCR1:

EIM_CS0GCR2: EIM_CS0RCR1:EIM_CS0RCR2: EIM_CS0WCR1: EIM_CS0WCR2的值应该是多少。

那么在我的应用程序当中,我应该用那种方式读写FPGA中的RAM。

0 件の賞賛
返信
3 返答(返信)

1,981件の閲覧回数
ruiguo
Contributor II

你好

我现在也在使用emi和fpga进行总线通信,读取fpga内部的数据,但是我现在遇到了一些问题,通过dma进行数据传输的时候,总线上没有任何信号发生,不知道你是否把这个通信测试成功,如果成功的话,非常希望你能给予我一定的帮助,非常感谢

郭瑞

0 件の賞賛
返信

1,981件の閲覧回数
jianminli
Contributor I

Hello rui guo

    I'm doing the same working now , it seems that u have realised the function connecting EIM to FPGA, can u give me some help?

0 件の賞賛
返信

1,980件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shan

please try eim settings as in attached sdk example.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信