Reading clock rate value and the actual measured value are differenc for the LVDS clock signal on Yocto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading clock rate value and the actual measured value are differenc for the LVDS clock signal on Yocto

2,404 Views
charleshuang
Senior Contributor II

I refer to the following URL.

Reference URL: https://community.freescale.com/thread/306801

I set a frequency of 29.5 MHz for the PLL5 LVDS clock signal on Yocto 3.10.17.1.0.2, the value is close to 29.5 MHz by oscilloscope.

But the clock rate value of pll5 video is close 206.5 MHz on console log.

Console log:

# cat /sys/kernel/debug/clk/osc/pll5_video/pll5_post_div/pll5_video_div/clk_rate

206499990

#  cat /sys/kernel/debug/clk/osc/pll5_video/pll5_post_div/pll5_video_div/ldb_di0_sel/clk_rate

206499990

Can you tell me why reading clock rate value and the actual measured value are difference?

Thank you.

Best Regards,

Alex Cheng

Labels (2)
0 Kudos
Reply
3 Replies

1,839 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Which modifications did you perform?

Can you provide the details?

Best Regards,

Alejandro

0 Kudos
Reply

1,839 Views
charleshuang
Senior Contributor II

Hi Alejandro,

I modify two files.

1) File: arc/arm/mach-imx/clk-imx6q.c. In imx6q_clocks_init():

/* ipu clock initialization */

-  init_ldb_clks(pll2_pfd0_352m);

+ init_ldb_clks(pll5_video_div);

2) File: drivers/video/mxc/ldb.c. Add a new mode in ldb_modedb[ ]:

static struct fb_videomode ldb_modedb[] = {

#ifdef CONFIG_ARCH_ADVANTECH

  {

  "LDB-XGA", 60, 1024, 768, 15385,

  220, 40,

  21, 7,

  60, 10,

  0,

  FB_VMODE_NONINTERLACED,

  FB_MODE_IS_DETAILED,},

+         {

+         "LDB-VGA", 60, 640, 480, 25175,

+          220, 40,

+           21,  7,

+           60, 10,

+            0,

+          FB_VMODE_NONINTERLACED,

+          FB_MODE_IS_DETAILED,

+         },

{

  "LDB-WXGA", 60, 1360, 768, 14148,

  158, 1,

Can you tell me why reading clock rate value and the actual measured value are difference?

Thank you.

Best Regards,

Alex Cheng

0 Kudos
Reply

1,839 Views
jim_lin
NXP Employee
NXP Employee

the correct path to read LVDS clock is:

/sys/kernel/debug/clk/osc/pll5_video/pll5_post_div/pll5_video_div/ldb_di0_sel/ldb_di0_div_7# cat clk_rate

FYI~

0 Kudos
Reply