Read CPU temperature in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Read CPU temperature in u-boot

跳至解决方案
4,050 次查看
ko-hey
Senior Contributor II

Hi all

My customer is using i.MX6S and L3.10.17.

I want to check whether the value changes or not when I changed TEMPERATURE_HOT parameter in soc.c.

Does i.MX6's register change when user changed TEMPERATURE_HOT parameter in soc.c ?

I guess that it will change the value of TEMPERATURE_HOT when user changed TEMPERATURE_HOT parameter in soc.c.

Am I correct ?

If my understanding is wrong, is it just reading the value of the temperature sensor?

Ko-hey

Original Attachment has been moved to: soc.c.zip

标签 (3)
0 项奖励
回复
1 解答
3,076 次查看
BiyongSUN
NXP Employee
NXP Employee

It  is to set a hot point to  compare to the value gets from thermal sensor, to decide in the uboot stage if the temperature if it is fine for boot to  the next stage here is linux.

 

void check_cpu_temperature(void)
{
int cpu_tmp = 0;

cpu_tmp = read_cpu_temperature();
while (cpu_tmp > TEMPERATURE_MIN && cpu_tmp < TEMPERATURE_MAX) {
if (cpu_tmp >= TEMPERATURE_HOT) {
printf("CPU is %d C, too hot to boot, waiting...\n",
cpu_tmp);
udelay(5000000);
cpu_tmp = read_cpu_temperature();
} else
break;
}
if (cpu_tmp > TEMPERATURE_MIN && cpu_tmp < TEMPERATURE_MAX)
printf("CPU:   Temperature %d C, calibration data: 0x%x\n",
cpu_tmp, fuse);
else
printf("CPU:   Temperature: can't get valid data!\n");
}

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,077 次查看
BiyongSUN
NXP Employee
NXP Employee

It  is to set a hot point to  compare to the value gets from thermal sensor, to decide in the uboot stage if the temperature if it is fine for boot to  the next stage here is linux.

 

void check_cpu_temperature(void)
{
int cpu_tmp = 0;

cpu_tmp = read_cpu_temperature();
while (cpu_tmp > TEMPERATURE_MIN && cpu_tmp < TEMPERATURE_MAX) {
if (cpu_tmp >= TEMPERATURE_HOT) {
printf("CPU is %d C, too hot to boot, waiting...\n",
cpu_tmp);
udelay(5000000);
cpu_tmp = read_cpu_temperature();
} else
break;
}
if (cpu_tmp > TEMPERATURE_MIN && cpu_tmp < TEMPERATURE_MAX)
printf("CPU:   Temperature %d C, calibration data: 0x%x\n",
cpu_tmp, fuse);
else
printf("CPU:   Temperature: can't get valid data!\n");
}

0 项奖励
回复
3,076 次查看
ko-hey
Senior Contributor II

Could someone follow and answer this question ?

Ko-hey

0 项奖励
回复