Re-programming of the PMIC in the SCM SoloX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re-programming of the PMIC in the SCM SoloX

785 次查看
erezamir
Contributor II

Hello,

We have the EVB of the SCM-I.mx6SX.
In order to boot from the serial downloader (OTG USB) there is a need for 5V supply. We do not want to use an external supply of 5V, instead use the internal SWBST of the PMIC.
The PMIC is pre-configured with SWBST_SEQ set to 0 so the SWBST does not turn on by default.
We re-programmed the PMICs OTP fuses to enable the SWBST to turn on, and SWBST turns on as expected.
We read the OTP_ECCI bit and it indicates an error (OTP_ECCI=1) .
The appnote (AN4536) specifies that if the OTP_ECCI bit is 1 - the part should be rejected.

Can you please clarify what should be done in this situation?
Is there any guidlines how to re-program a PMIC which was pre-programmed?

Thanks,

标签 (3)
0 项奖励
回复
0 回复数