Re: mfgtool imx8mq evk fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: mfgtool imx8mq evk fails

362 Views
tmapes
Contributor I

I'm having the exact same problem on my machine.  I believe the problem is that the file "rootfs.tar.bz2" is zero bytes in length.  It looks like the rootfs didn't get zipped properly.

0 Kudos
1 Reply

331 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Use "mfgtools-with-rootfs-mx8.zip" instead of "mfgtools-without-rootfs-mx8.zip".


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos